This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 with RS-422 (Hardware Question)

Other Parts Discussed in Thread: MSP430FR5969

Hello,

I am using a msp430fr5969 board. I need to communicate with a Airmar 150wx unit to receive serial strings. The Airmar uses RS-422 communication protocol. If i am correct in interpreting how that works it will send a maximum differential voltage of -6 to +6 volts to the Rx and Tx pins on the board. I think the pins have a maximum input of 4.2 volts but I am not sure. 

Can someone confirm whether or not the board Rx and Tx pins could  handle signals sent at the levels from Rs-422? If not, does any one have a suggestion of to make this work?

Thanks,

Nolan 

**Attention** This is a public forum