I know nothing about TI microcontrollers. I need a computer that is at least 16 bit if not 32 bit, 128k to 256k flash, as much ram as possible, von neuman architecture, stack based, with peripherials such as SPI, I2C, UART, ADC, Counter/Timers, etc. To be used in an application that has an RTOS, file system, etc. I am posting here to get the help of TI experts who could suggest a TI processor that would fill this bill. Does not have to be micro power. Will most likely have a 12V gel cell with either connection to 110 VAC OR SOLAR. Thanks. Alvin....