Communication on UART line triggers noise in nearby capacitive touch lines in MSP430G2755
All lines are used in the 40 pin micro,so the touch switches cannot be re-alligned away from the uart line
The UART baudrate is decreased from 1Mhz to 9600Hz which gave a significant decrease in the noise induction on the touch lines.
Compromising the sensitivity is done to further reduce the noise.
But still there is a chance of noise on the touch lines and the miss triggering of the capacitive touch switches happens
Is there any hardware/software design solution to reduce the noise.