This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debug error: MSP430: GEL: Encountered a problem loading file: [filepath].out Could not open file



I am writing an assembly project for the MSP 430 in CCS and if I uncomment a line of code that has a #VALUE which is defined earlier as VALUE    .equ    BASEVALUE*3 then I get the error in the title.  If I comment that line out the code runs fine.  What's going on?

**Attention** This is a public forum