This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C eeprom Acknowledgement not working

Other Parts Discussed in Thread: MSP430F169

Hi,

I am trying to implement the i2c eeprom communication using the application note SLAA208 . The acknowledgement polling given in the source code is not working, If I use the acknowledgement polling data writing to eeprom doesn't write to eeprom, instead if I give a time delay of 4 to 6 ms between writes, it works fine, can somebody help me with correct implementation of acknowledgement polling.

Regards,

Sivaram

**Attention** This is a public forum