Hello all,
I am attempting to work with a Flash Memory chip, and have so far only had negative results. I am attempting to work with the MSP430FR5728 by TI, and the S70FL01GS by Spansion.
I am trying to perform the Read ID, however all of my attempts have resulted in either FFh or 00h.
I have been using a logic analyzer to see the results, and will post a screenshot below:
For the life of me I am not sure what I am doing wrong. I have read through the datasheets, and made sure the voltages and configurations matched that of what was needed. I even made sure that the circuit was wired correctly, as can be seen in the figure below.
I believe that everything is wired correctly for this simple task of Read ID. Below is also the code I wrote using IAR Embedded Workbench
/***********************************************************
Code Goal: Write a Byte of data to address of S70FL01GS.
After which, read the same address to prove that the
data byte was properly recorded to the Flash Memory.
Read ID: Datasheet says send command and then 3 dummy bytes
Write: Datasheet states need to Enable Write, send 3 address
bytes, and requires the READ FLAG STATUS REGISTER command being
issued with at least one byte output.
Read: send 3 address bytes of where want to read
Program: IAR Embedded Workbench IDE
MCU: MSP430FR5728
SPI: B0 mode selected from device
UCB0SIMO: P1.6
UCB0S0MI: P1.7
UCB0CLK: P2.2
CSn 1: PJ.2
CSn 1: PJ.4
***********************************************************/
#include "string.h"
#include "msp430.h"
#include <stdio.h>
char b1 = 0x01; // Flash Addr Part 1 for Write
char b2 = 0x02; // Flash Addr Part 2 for Write
char b3 = 0x01; // Flash Addr Part 3 for Write
char b4 = 0x01; // Flash Addr Part 1 for Read
char b5 = 0x02; // Flash Addr Part 2 for Read
char b6 = 0x01; // Flash Addr Part 3 for Read
char Q;
char T;
unsigned char RXData =0;
unsigned char TXData;
char Readout[20];
/***************************************************
Flash Code
***************************************************/
char FlashByte(char S){ // General FlashByte Transmit
__delay_cycles(60);
UCB0TXBUF = S;
while (!(UCB0IFG & UCTXIFG));
S = UCB0RXBUF;
while (!(UCB0IFG & UCRXIFG));
return S;
}
char FlashComID(char S){ // Read ID command 9Fh
PJOUT &= ~ BIT4;
//while (!(UCB0IFG & UCTXIFG));
UCB0TXBUF = S; // Send Command
while (!(UCB0IFG & UCTXIFG));
while (!(UCB0IFG & UCRXIFG));
UCB0TXBUF = 0x00; // Dummy 1
while (!(UCB0IFG & UCTXIFG));
Readout[0] = UCB0RXBUF; // Read 1
while (!(UCB0IFG & UCRXIFG));
UCB0TXBUF = 0x00; // Dummy 2
while (!(UCB0IFG & UCTXIFG));
Readout[1] = UCB0RXBUF; // Read 2
while (!(UCB0IFG & UCRXIFG));
UCB0TXBUF = 0x00; // Dummy 3
while (!(UCB0IFG & UCTXIFG));
Readout[2] = UCB0RXBUF; // Read 3
while (!(UCB0IFG & UCRXIFG));
PJOUT |= BIT4;
return (UCB0RXBUF);
}
/***************************************************
Main Code
***************************************************/
int main(void){
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
PJDIR |= 0x1F;
PJOUT |= 0x1F;
// Clock Setup For SPI
CSCTL0_H = 0xA5;
CSCTL1 |= DCOFSEL0 + DCOFSEL1; // Set DCO = 8MHz
CSCTL2 = SELA_3 + SELS_3 + SELM_3; // set ACLK = SMCLK = MCLK = DCO
CSCTL3 = DIVA_1 + DIVS_1 + DIVM_1; // ACLK = SMCLK = MCLK = 1MHz
// Configure SPI
P1SEL1 |= BIT6 + BIT7; // Set pins for primary purpose
P2SEL1 |= BIT2; // Set pin for primary purpose
UCB0CTLW0 |= UCSWRST;
UCB0CTLW0 |= UCCKPH + UCMST + UCSYNC + UCMSB;
UCB0CTLW0 |= UCSSEL_3; // SMCLK = 4MHz
UCB0BR0 = 0x02; // /2
UCB0BR1 = 0; //
UCB0CTLW0 &= ~UCSWRST;
for(;;){
FlashComID(0x9F);
__delay_cycles(500);
}
}
Anyone have any ideas of what I might be doing wrong? Suggestions?
Thanks!