I'm planning on starting developing with this launchpad and booster but the user guide suggests that the sample code is too big for the free CCS - I'm a bit confused as there seem to be mixed messages. Is it just the full sample (with multiple programs running inc. game, temp sensor, clock etc) that takes over the 16K limit so I can recompile ok for reduced function - although it says that CCS sample code is locked for edit???
Could someone from the FRAM launchpad team please help to clarify the situation as I can't afford the $700+ for the full version at the moment (this is an amateur development that may go into production if successful)
Thank you
Colin