Also, I do not have the the \arm folder under C:\ti\ccsv6\ccs_base. I tried to run the same example under could CCS, I get the following
"../lab4_adc14.c", line 99: error #20: identifier "ADC14SSEL__1" is undefined >> Compilation failure "../lab4_adc14.c", line 106: fatal error #35: #error directive: "Add code line to configure A15 ADC input selection for MEM0 with VREF=AVCC" 1 error and 1 catastrophic error detected in the compilation of "../lab4_adc14.c". Compilation terminated. gmake: *** [lab4_adc14.obj] Error 1 gmake: Target `all' not remade because of errors. **** Build Finished ****