This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

poor duty cycle of clock

Other Parts Discussed in Thread: MSP430F5529

Hi,

I am using SPI on USCB1 port of MSP430F5529 LP. i am setting the FLL to stabilize at 24MHz and want to use SPI to write SDHC card at 24MHz frequency. I am unable to get proper clock beyond 4Mhz. Between 2MHz and 4MHz the SCLK cycles are proper in number but poor on duty cycles. 

Below 2Mhz i get a very good SCLK. beyond 4MHz I dont get the proper clock cycles also - some times I see only 2 or 3 clock cycles and never 8 clock cycles. 

I am at a loss to find a reason and solution to this. Need help.

Regards

Viney Chaddha

**Attention** This is a public forum