MSP430G2755, CCS 6.1.0.00104. Global symbols that are static, and global arrays do no show up in the .map file. I can have a global array Counts[10] and in the .map file it says I have 2,174 bytes of ram free; I can change it to Counts[1000] and it will still say I have 2,174 bytes free. I cannot find anything in the linker properties that looks like it would suppress this info.
???
Thanks, Doug