Message from customer:
"As for the problem with our
computers, it seems it is related to our specific tablet PCs that we use.
They are HP tablet PCs and the USB driver for the emulator USB stick seems to
be the problem. I have tried this on 3 machines so far. 2 of the
were running Windows XP and one was running Windows 7, all are 32-bit
installs. The message we get when we try to program the Chronos is:
"Error initializing emulator: Could not initialize device interface"
Actually, now with the Windows 7 tablet once the USB programmer is plugged in
it will hard freeze the machine up. I am very worried because I have 45
of these tablets that we use for the class and the only thing that works is the
RF access point, the TI Control Center, and running CCS, no programming the devices.
We have set up a couple other machines that work fine, so we know the problem
is the laptops. Something about the chipset or something. "