Other Parts Discussed in Thread: MSP430F6779, MSP430F67791
HI,
I am starting now with a e-meter project with the MSP430F6779.
I am searching for an overview of all the registers used in it and wanted to ask if there is something like that, since I didn't find it in the datasheet.
It should look like this:
SD24B Interrupt Enable Register (SD24BIE)
Bit 0: SD24B Channel 0 Interrupt Flag (SD24IFG0)
1 when input on channel 0
0 when no input
Bit 1: SD24B Channel 1 Interrupt Flag (SD24IFG1)
...
Bit 2: ...
I used the msp430f67791.h for the example.
It doesn't have to be specifically for the MSP430F6779 since I guess I would look alike on every one of the microcontrollers.