This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-Gang Programmer Standalone Mode

Other Parts Discussed in Thread: MSP-GANG

Hi,

I am using MSP Gang Programmer.

In this Interactive Mode is working fine with Memory Options. (I want only main memory to be programmed)

In Standalone mode: 

It is erasing All memory then programming , also no option for setting memory options as erase main memory specificaly in Standalone mode.


please help.

  • Hi Nesh,

    Can you answer the following questions so that we can try to diagnose your issue?

    1. Can you please let us know which MSP-GANG firmware version you are using? (Go to About > About)
    2. Can you show us the Memory options that you have selected in interactive mode?
    3. In standalone mode, are you telling the MSP-GANG to use the same image stored in the MSP-GANG memory, that you generated in interactive mode?
    4. Please provide detailed steps of how to test and reproduce the issue, so that we can recreate it here on our side. What addresses should already have data in them for example, which addresses do you expect to be erased vs preserved, etc.

    Regards,
    Katie

  • Hi Nesh,

    Any update - are you still having the issue or have information you can provide as asked above?

    -Katie
  • I'm going to close the thread due to inactivity, but please post back if you continue to have problems or have answers to my information request above.
    -Katie

**Attention** This is a public forum