Hello,
A while back I posted a question about safeguarding firmware in far-east manufacturing. The conclusion seemed to be that the best approach is to give the binary file to a trusted vendor of the chip, so that they can pre-program it. The pre-programmed chips can then be delivered to the (not necessarily trusted) PCB assembly company with the security fuses burned out: https://e2e.ti.com/support/microcontrollers/msp430/f/166/p/323810/1127161#1127161
I'm at the point now when I would like to order a test batch of 1000 pre-programmed chips. Specifically the model number of the chip I am using is MSP430G2332IPW20. I've checked Digikey, Farnell and Arrow for pre-programming services but couldn't find any. Am I missing something? Should I instead be approaching a local (in my case, British) PCB assembly company rather than an actual vendor? I'd rather work with someone's who's actually done this before. Surely it's a pretty standard service?
I'd be grateful for any links/contacts to companies either in the UK, or in the Pearl River Delta area of South China, that offer such a service. I haven't checked the rules for this forum, so am not sure if you're allowed to promote specific companies here. If this is the case, then I would be grateful if you would message me privately. Otherwise, please post here as no doubt this is valuable information for anyone seeking a similar solution.
Many thanks in advance for any help you can offer. Best,
Ed