Other Parts Discussed in Thread: MSP430F2618
Hey Team,
I am looking for a MCU with two DACs and I2C.
Preferably one that can meet the following specs:
- 8 to 16 GPIO ports.
- at least 2 DACs. Prefer 10 bits, but can settle for 8 bits.
- May want an ADC, but that is optional.
- If it has a good built-in temp sensor that would be a bonus.
- I2C interface should run off 1.8V, but the DACs need to run off 3.3V.
- smallest package possible.
I have come across the MSP430F2618. Are there other options with dual DACs?
Thanks for the help!