Other Parts Discussed in Thread: ENERGYTRACE
I cant found informations about EnergyTrace MSP432 LaunchPad maximum current value ?
Anybody knows ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ENERGYTRACE
I cant found informations about EnergyTrace MSP432 LaunchPad maximum current value ?
Anybody knows ?
Lukasz,
I don't know if it is the right answer, but in this thread

it says "Target current exceeded with the maximum current (75mA) supported by EnergyTrace."
Dennis
Hi Lukasz.
I found this from SLAU597A - MSP432P401R LaunchPad™ Development Kit User's Guide
2.4.1 XDS110-ET USB Power
The most common power-supply scenario is from USB through the XDS110-ET debugger. This provides
5-V power from the USB and also regulates this power rail to 3.3 V for XDS110-ET operation and 3.3 V to
the target side of the LaunchPad. Power from the XDS110-ET is controlled by the isolation block 3V3
jumper, ensure this jumper is connected for power to be provided to the target MCU side.
Under normal operation, the LDO on the XDS110-ET can supply up to 500 mA of current to the target side
including any BoosterPacks plugged in. However, when debugging and using the EnergyTrace technology
tool, this current is limited to 75 mA total. Be aware of this current limitation when using EnergyTrace
technology.
**Attention** This is a public forum