Hi,
We purchased TI Development board MSP-TS430PEU128 for developing energy meter of class 0.2 accuracy using MSp430F6779A or MSP430F6765A
The reason for deciding these controllers for this project was to utilize ready made Energy Libraries (emeter) from TI for getting Energy values. However, when I download the MSP430 Energy Library from I do not find libraries for these controllers. Library was available for few controllers .From the MSP430F6x series , emeter library is available for Msp430F6736 .
The documentation SLAA538.pdf mentions the following:
"This application report describes how to execute the Texas Instruments MSP430 Energy Library, which
uses a common set of source files to support meters based on the MSP430FE427A, MSP430F47197,
MSP430F4794, MSP430F6736, and MSP430AFE253 devices. This application report includes the
necessary information about the APIs of the energy library.The MSP430 Energy Library is available here:........
Does this mean that no emeter library support for MSp430F6779A or MSP430F6765A from Texas Instruments?
Where can I find the Energy libraries for MSp430F6779A or MSP430F6765A ?
Can anybody help me in converting the emeter-toolkit-6736 to emeter-toolkit-6779A?
Best regards,
Kush