I have everything set to set the P4IFG.5 and P4IFG.6 including releasing the LOCKLPM5 bit at the right time.
Problem: The flag is not set in the P4IV and interrupt is not noted when the button is pushed.
I have checked my hardware, and the two buttons are at 3.31V from the pullup in the pin on the MSP430FR5969. When the button is pushed, the value is driven to 0.0V which should signal an interrupt for my falling edge detect.
I have the following code configuration and operation code:
CONFIGURATION:
P4DIR &= ~(BIT7 + BIT6 + BIT5 + BIT4); // Direction = input (0); output would be (1)
P4DIR |= BIT3 + BIT2 + BIT1 + BIT0; // Set Port4 pins to output function
P4REN |= BIT7 + BIT6 + BIT5 + BIT4; // Enable pull-up/pull-down resistor // ALIGN WITH EDGE DETECT
P4OUT |= BIT7 + BIT6 + BIT5 + BIT4; // Configure pull-up = 1; pull-down = 0; 1 used for high to low interrupt
P4OUT &= ~(BIT3 + BIT2 + BIT1 + BIT0); // Zero(0) for pull-down on N/C pins.
// P4SEL0.x and P4SEL1.x = 00b is for I/O configuration
// Pins P4.3 - P4.0 are output Enable pins
P4SEL0 &= ~(BIT7 + BIT6 + BIT5 + BIT4);
P4SEL0 &= ~(BIT3 + BIT2 + BIT1 + BIT0); // Set to primary function (00b -- per channel)
P4SEL1 &= ~(BIT7 + BIT6 + BIT5 + BIT4);
P4SEL1 &= ~(BIT3 + BIT2 + BIT1 + BIT0); // Set to primary function (00b -- per channel)
P4IES |= BIT7 + BIT6 + BIT5 + BIT4; // P4.7, P4.6, P4.5 and P4.4 Hi to Lo falling edge interrupt (1b) //CONFIRMED
// Lock bit is cleared:
PM5CTL0 &= ~LOCKLPM5;
P4IFG &= ~(BIT7 + BIT6 + BIT5 + BIT4 + BIT3 + BIT2 + BIT1 + BIT0); // Clear Port 4 Interrupt Flags
P4IE |= BIT7 + BIT6 + BIT5 + BIT4; // P4.7, P4.6(B1), P4.5(B2) and P4.4 interrupts enabled
OPERATION CALL:
// Waiting for button press (code is stuck here with no IFG):
__bis_SR_register(LPM1_bits | GIE); // Enter LPM1 for Timer0_B7 w/interrupt
__no_operation(); // For debugger happiness
// Interrupt set up (never entered):
#pragma vector=PORT4_VECTOR
__interrupt void PORT4_ISR_HOOK(void)
{
/* USER CODE START (section: PORT4_ISR_HOOK) */
switch(__even_in_range(P4IV, P4IV_P4IFG7))
{
case P4IV_NONE: break; // Vector 0: No interrupts pending;
case P4IV_P4IFG0: break; // Vector 2: P4IFG.0;
case P4IV_P4IFG1: break; // Vector 4: P4IFG.1;
case P4IV_P4IFG2: break; // Vector 6: P4IFG.2;
case P4IV_P4IFG3: break; // Vector 8: P4IFG.3;
case P4IV_P4IFG4: break; // Vector 10 (0xA): P4IFG.4;
case P4IV_P4IFG5: // Vector 12 (0xC): P4IFG.5;
ButtonPress = BUTTON2PRESSED; // BUTTON2PRESSED;
P4IFG &= ~BIT5; // Clear P4.5 IFG
break; // end Vector 12: P4IFG.5;
case P4IV_P4IFG6: // Vector 14 (0xE): P4IFG.6;
ButtonPress = BUTTON1PRESSED; // BUTTON1PRESSED;
P4IFG &= ~BIT6; // Clear P4.6 IFG
break; // end Vector 14: P4IFG.6;
case P4IV_P4IFG7: break; // Vector 16 (0xF): P4IFG.7;
default: ButtonPress = 0; break; // Default to NOBUTTONPRESSED condition
}
/* Exit Low Power Mode before return from interrupt */
__bic_SR_register_on_exit(LPM1_bits | GIE); // Exit LPM1 | GIE
/* USER CODE END (section: PORT4_ISR_HOOK) */
}
******************************************************************************************
I can set the IFG flag with this command just before the __bis_SR_register(LPM1_bits | GIE) command:
P4IFG |= BIT5;
and the interrupt works.
QUESTION: What am I missing?
Thanks.