Hey, i am again xD
i worked a bit with ADC (i need 18 channel input), one pin has with no external voltage always reference voltage, maybe this port crashed?
On other pins, if i take an external voltage and the value overstep ~1,3 V the current increase untile 0,1 A and more, did i crashed the mc ?
Additional i got very high temprature :( i change my source only use _sleep() in main and timer32 Interrupt an i got 72°C, i changed the board and i only got 50 °C...