Ok I have searched enough and I can't find the reason why this apparently simple task is not behaving as expected
I dont want to go to a LPM state but I want to save as much power as possible, so I would like to source MCLK and ACLK from LFXTCLK something like this:
But I can not get the DCO to shutdown. So far I have this test program
int main (void)
{
WDTCTL = WDTPW + WDTHOLD + WDTSSEL; //Stop watchdog and even source it from ACLK
BCSCTL1 = XT2OFF | 4; // XT2Off, set the DCO RSELx
BCSCTL2 = SELM_3 | SELS | DIVM_3; // MCLK source is LFXTCLK and Divide MCLK
__bis_SR_register(SCG0|SCG1); // This should shutdown the DCO
while(1); // Just wait
}
My guess would be that this code should shutdown the DCO. The Configurations are practically the same as in the picture. However if I change the value of RSEL (DCO frequency) and then measure the current it changes acordingly, that indicates that the DCO is still ON, I have checked the peripherals and no one should be using the the SMCLK, there is no XT2 in my circuit, so I don't know if that is a problem as SMCLK can only be sourced from DCO or XT2...
The DCO is only off when the CPUOFF bit is also set, am I doing something wrong here?
(Side note, in the user guide ( www.ti.com/.../slau144 ) page 278 what is XSELM1 shouldn't it be SELM1? Have I found a bug in the documentation while looking for an answer on this:P)