Hello,
i'm searching for a simple wireless mesh network based on sub-ghz (868MHz) technology for simple 3 phase energy monitoring.
i've found a solution from 2011 wich demonstrates CC430 with Singe phase Energy Monitoring directly with a CC430 MCU.
My questions are:
1. If the MCU is connected to 230V AC mains with only a few 2 MOhm resistors, is it allowed to provide an external SMA connector for antenna conection?
This connector would have no isolation to mains, because it is also connected to the mcu and the metering circuit.
2. if it needs galvanic isolation between SMA Antenna connector and metering circuit, is it possible to use a normal MSP430 MCU with
ADuM (ISOpower SPI isolator with on chip DC/DC converter from Analog Devices) and extra RF Chip?
MSP430 <-> ADuM <-> RFChip CCxx <-> SMA Antenna connector
3. Wich MCU can be used for 3 Phase Energy Metering (6x 12Bit ADC) + RF mesh networking for up to 1k nodes.
All nodes will be accessed every 10 minutes.