Other Parts Discussed in Thread: MSP430G2553, ENERGIA
It was working, but not anymore.
I am taking a class at Edx, computer interfaces and building a robot based on the MSP430G2553 launchpad. I was using Energia 1.6 to install a class sketch. It, the sketch, was not working correctly. I tried to revert to the previous sketch to see if I messed up the bread board which has the components used by the MSP. Energia will not install the older sketch (which it had installed OK the day before). Looking for answers to the error message (No unused FET found) when it tried to install on COM1 (Windows 7) I found some hints but re-installation as Admin for the XDS110 did not solve it. 15 minutes before this I had installed the newer sketch on COM3 with no problems. COM3 is gone. So is Other Devices section in Device Manager. No clue where they went. I tried to reinstall the XDS110 drivers, no change even though it says OK. Power cycle the system, off for an hour, no change.
When I initially did the install I had to do it twice to get the drivers to install OK. That worked fine for three weeks. It just 'broke' today, and I have no clue where to go for a resolution. I would uninstall it if I knew where to try that and then reinstall.