Other Parts Discussed in Thread: MSP430F2416, MSP430F2419
Hi,
I am using MSP430F2416 i have developed the schematic as per the MSP-TS430PM64 target board circuits.
(1) While i try to flash the code i am getting the following error if 3.3v connect external supply "LOAD PROGRAM ERROR". I have attached the screen shot of this error for your verification in this "Load program error" files.
(2) If i 3.3V external supply removed, the above error has been rectified and the program can be flashed to the uC. After that if i connected 3.3V external supply to the controller then it not responding while debugging the program the following error occurred.
"MSP430: Trouble Halting Target CPU: Internal error"
The attached " Halting error" file shows the screen shot of this error.
I am suspecting whether the controller is alive or not.
Thanks in advanceLoad progrm error.docHalting error.doc