This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm having my board which is based on MSP430i2041. I'm working with energy metering code. I'm reading parameters for AC signal like Irms, Vrms, Mains Frequency etc. I can see the correct the value of Irms, Vrms but I'm always geeting zero value for Mains frequency, active power. What can be the reason?
Thanks,
Abhay
Abhay,
There can be many cause of this, there is not enough information for me to analyse the cause. Which code and hardware are you using ? Did you modify something in the reference code ? Please provide me more information to proceed.
mars
Hi Mars,
I'm using MSP430i2041 based hardware. IT is similar to the that of EVM based on the same processor. Also I'm using energy metering code provided on TI webpage of EVM.
I will provide some background - Initially we were not getting proper readings for Irms (values were all over the place), but I was getting correct mains frequency. We corrected our hardware and then we started getting correct values of Irms but at the expense of mains frequency (which is zero always).
If I try the same code with EVM, it gives proper reading for mains frequency. So is there some problem in our hardware which is causing this behavior with mains frequency. But then I should not get the Irms or Vrms as mains frequency is calculated from these signals.
Thanks,
Abhay
Ahbay,
That sound strange. Can you share your schematic you are using ? Thank you.
mars
**Attention** This is a public forum