This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPFlasher -i option issues



I am using MSPFlasher application version 1.03.07.00  on Linux.  I am running an automated hardware in the loop system with multiple programmers so I require use of the "-i" option to specify connection port.

It does not handle the -i option correctly (i.e. "-i /dev/ttyACM3").

Doing some quick debug it appears there are two issues:

1) The passed argument is capitalized at some point which causes an issue when compared against "ttyACM".

2) After I hacked #1 I found another problem.  Per the documentation the argument should be passed in the form "/dev/ttyACM0", but it only seems to work for "ttyACM0".

Hoping these issues can be addressed in the next release.

Thanks.

**Attention** This is a public forum