Hi there,
i am using DMA to send and read to the SPI RX and TX Buffer.
This works very well but if i want to use SPI directly without the DMA it doenst works.
I used the SPI before i assigned it to the DMA and it works well, but when i use it after assigning it to the DMA i cant send and read anything.
I try shut down the DMA module and disable the channels, do i have to disatached the send and received DMA buffer with the SPI?