Other Parts Discussed in Thread: MSP430FR5738, MSP430FR5734, MSP430FR5969, MSP-EXP430FR5969, MSP-EXP430FR5739
I am trying to debug an external FR5738 connected to an FR5969LP via the .05" jumper header to the EZ430 emulator on board. This has worked fine on other launchpads, and it is able to program and debug a separate G2332 just fine. However, when I try to program the FR5738, it says
"Error connecting to the target:
The target setup (MSP430FR5738) does not match the actual target type (MSP430FR5734)"
Now I am definitely using an FR5738. I tried making a new project, reloading the linker command file, rebuilding the target config, etc, and none of that worked. I was able to successfully program the chip by changing the target config and linker command file to the FR5734, which is what it appears to think the target is. This solution is not satisfactory, however, because the 5734 has half the program memory of the 5738.
Any thoughts on a way to fix this?
Thanks!
Brody G