This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Timer PWM Example

Other Parts Discussed in Thread: CC430F5137

Hello i am using the CC430f5137. I am using the example for generating the PWM but i can not get it that how total period becomes 233us when i used the clock of 1 MHz. Below is the code taken from example of ti.

*******************************************************************************
// CC430F513x Demo - Timer_A3, PWM TA1.1-2, Up/Down Mode, DCO SMCLK
//
// Description: This program generates two PWM outputs on P2.2,3 using
// Timer1_A configured for up/down mode. The value in CCR0, 128, defines the
// PWM period/2 and the values in CCR1 and CCR2 the PWM duty cycles. Using
// ~1.045MHz SMCLK as TACLK, the timer period is ~233us with a 75% duty cycle
// on P2.0 and 25% on P2.2.
// SMCLK = MCLK = TACLK = default DCO ~1.045MHz.
//
// CC430F5137
// -------------------
// /|\| |
// | | |
// --|RST |
// | |
// | P2.0/TA1.1|--> CCR1 - 75% PWM
// | P2.2/TA1.2|--> CCR2 - 25% PWM
//
// M Morales
// Texas Instruments Inc.
// April 2009
// Built with CCE Version: 3.2.2 and IAR Embedded Workbench Version: 4.11B
//******************************************************************************

#include <msp430.h>

int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT

PMAPPWD = 0x02D52; // Get write-access to port mapping regs
P2MAP0 = PM_TA1CCR1A; // Map TA1CCR1 output to P2.0
P2MAP2 = PM_TA1CCR2A; // Map TA1CCR2 output to P2.2
PMAPPWD = 0; // Lock port mapping registers

P2DIR |= BIT0 + BIT2; // P2.0 and P2.2 output
P2SEL |= BIT0 + BIT2; // P2.0 and P2.2 options select

TA1CCR0 = 128; // PWM Period/2
TA1CCTL1 = OUTMOD_6; // CCR1 toggle/set
TA1CCR1 = 32; // CCR1 PWM duty cycle
TA1CCTL2 = OUTMOD_6; // CCR2 toggle/set
TA1CCR2 = 96; // CCR2 PWM duty cycle
TA1CTL = TASSEL_2 + MC_3 + TACLR; // SMCLK, up-down mode, clear TAR

__bis_SR_register(LPM0_bits); // Enter LPM0
__no_operation(); // For debugger
}

  • In up-down mode, the frequency is determined by twice the CCR0 number of ticks. 1 MHz / (2 × 128) = 256 µs, or 1.045 MHz / (2 × 128)  = 245 µs.

    I don't know why the comment says otherwise.
    In any case, the DCO is not very accurate to begin with. It's possible that somebody measured 233 µs with an oscilloscope; your own measurement would probably get some other value nearby.

  • MSP430s actually do not have Timers. The so-called Timers are actually Counters. Counters can be used as Timers if and only if an accurate clock is available for the Counters to count the time.

**Attention** This is a public forum