Other Parts Discussed in Thread: MSP430F1610
Hi,
I am trying to use XT1 clock in the following code snippet:
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer
P1DIR |= 0xff;
BCSCTL1 = XT2OFF | XTS;
BCSCTL2 = SELM0 | SELM1;
volatile unsigned int j;
do {
IFG1 &= ~OFIFG;
for (j = 0xff; j>0; j--);
} while((IFG1&OFIFG) == OFIFG);
The problem is that when I comment the do while loop, the code works fine with DCO clock. But when the I uncomment the do while loop, the code doesnot work with the XT1 clock. I am using MSP430F1610 and supplying an external frequency of 4MHz. The output of the function generator is directly connected to XT1 pin of MSP430F1610. I am using the normal blinking LED example with this external clock.
Any help is most appreciated ! Thanks in advance !