This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

setting up external clock MSP430FR5739



I’d like to setup so that the main clock runs from an external 24Mhz source on XIN pin.   I write CSCTL2 register to 0x0000 to select MCLK to XT1CLK.  I set CSCLT3 to 0x0000 so everything is divide by 1.  CSCT4 to 0xC1F0 to set XT1 Source from external clock in high frequency mode.  PJSEL1 to 0x30 to set enable the XIN/XOUT functions.   This doesn’t work so what more am I missing?    I’ve a feeling I’m violating a configuration rule that I’m not aware of or I’m missing an enable somewhere.  

  • Don't use numerical values when the register fields have proper symbols.

    You have to clear the fault flags; see section 3.2.7 of the User's Guide, and MSP430FR57xx_CS_03.c in the example C code package (SLAC491).

  • Sorry, I did clear the flags by writing CSCTL5 to 0x0000.
    PJSEL1 = 0x30;
    CSCTL2 = 0x0000;
    CSCTL3 = 0x0000;
    CSCTL5 = 0x0000;
    CSCTL6 = 0x0000;
    CSCTL4 = 0xC1F0;

    "Don't use numerical values when the register fields have proper symbols" - What does this mean?

    Do I have to write CSCTL0 first to enable access?
  • There are more fault flags. And it is not enough to clear them once; you have to wait until the fault condition actually goes away. (See the example code.)

    Nobody is going to reverse engineer what these numbers might mean; use symbols like XT2DRIVE_3.

  • I see what you mean about the reverse engineering. I mostly copied the code you suggested. I've simple code that what ever is on P2Bus shows up on P1 and P3 buses. it works when i do not try and change the MCLK from default. Now nothing happens and all busses are tri-state. Is there a restart or wait period needed when changing clock sources? Or is that what checking the fault flag does?

    PJSEL0 |= BIT4 + BIT5;
    CSCTL0_H = 0xA5;
    CSCTL1 |= DCOFSEL0 + DCOFSEL1; // Set max. DCO setting
    CSCTL2 = SELA_0 + SELS_3 + SELM_0; // set ACLK = XT1; MCLK = XT1
    CSCTL3 = DIVA_0 + DIVS_0 + DIVM_0; // set all dividers by 1
    CSCTL4 |= XT1DRIVE_3;
    CSCTL4 &= ~XT1OFF;

    do
    {
    CSCTL5 &= ~XT1OFFG;
    // Clear XT1 fault flag
    SFRIFG1 &= ~OFIFG;
    }while (SFRIFG1&OFIFG); // Test oscillator fault flag

    // Now that osc is running enable fault interrupt
    SFRIE1 |= OFIE;

    P3DIR = 0xFF; // bus is an output
    P2DIR = 0x00; // bus is an input
    P1DIR = 0xFF; // bus is an output;

    while(1)
    {
    P3OUT = P2IN;
    P1OUT = P2IN;
    __delay_cycles(1);
    }
  • Now XIN is not configured for bypass mode.

**Attention** This is a public forum