This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

A firmware update is required for the MSP430 Debug Interface



Hello All,

I'm getting a request to update my firmware for the MSP430. But after I update, and I try and debug it constantly fails with :

MSP430: File Loader: Verification failed: Values at address 0x0000000000000020 do not match Please verify target memory and memory map.

MSP430: GEL: File: "...path on local drive...file.out": a data verification error occurred, file load failed.

If I don't update the firmware and opt for the "Ignore" option, then the error message is the same.

Has anyone has anything similar to this and can advise?

Thank you in advance

  • I do have to update whenever i switch from CCS5.5, some of my older projects, and newer CCS6.1 version.

    But it just upgrades or downgrades, takes a bit of time but afterwards program do compile and debug without any issues.

    So i would suggest its your code?

    Did you try some very simple example codes with only a couple of code lines?

**Attention** This is a public forum