Other Parts Discussed in Thread: MSP430FR5969, MSP-EXP430FR5969, CC2650STK
I bought the MSP430FR5969 Launch Pad with Sharp96 Booster pack. Using IAR I built the 430BOOST-SHARP96-GRlibExample project with no problems. When I launch the code from main using the built in debugger it calls function GrFlush() then appears to do a reset. It doesn't get to the functions that write on the LCD screen below te above mentioned function in main(). Did this ever work?