I purchased the newer black MSP-FET tool and use with IAR tools. It is constantly asking to update the FET firmware and complains about setting the voltage, whether I power the device or the FET powers the device. The older MSP-FETU430IF does not have this problem. This is the message I get:
Using license: Standalone license - IAR Embedded Workbench for Texas Instruments MSP430 6.30
Firmware version 3.5.1.1
Interface dll version 0.0.65471.65535
Could not set device Vcc (Vcc) , voltage=0x9c4
Could not set device Vcc : (Close) , vccOff=0x1
Fatal error: Failed to set device voltage. Session aborted!
After this if I try again sometimes it will work, sometimes not. It does not matter whether I am programming my system (msp430f5659) or programming the same micro in the MSP-TS430PZ100USB development board. Or even if I use with other processors (msp430f5528, msp430f5310, msp430fr5849, ...). The older FET works everytime. The newer FET is frustratingly unreliable.