Other Parts Discussed in Thread: MSP430F5438A
Hi, I am using MSP430F5438A and learning about accelerometer interfacing. I am trying to do the single axis tilt meter using ADXL335B.
Wixey tilt meter:
The thing is that wixey digital gauge has following specs.
Range: +/- 180 degrees
Resolution: 0.1 degrees
Accuracy: +/- 0.2 degrees
How can I specify my system in the same way as wixey did ? I tried the following approach. Please tell me that am I on the right track.
The thing is that I am using ADXL335B with 12 bit ADC. My power supply is 3.3V and Aref = 5V. I am doing single axis tilt calculations.
The data sheet of the sensor is as follows
http://www.analog.com/media/en/technical-documentation/data-sheets/ADXL335.pdf
My calculations are as follows
Desired Range = 0 to 180 degrees.
1. ) Resolution : 3.3 / 4096 = 0.8 mV
2.) ADC_out = ((3.3) / 5 ) x 4096= 2703.36
3) (1.99-1.65) = 0.34 ; 1.99 corresponds to 90 degree and 1.65 V correspond to 0 degree.
0.8mV / 90 = 0.008 mV / degree
But i am lost here. what is the angle resolution in degrees?
How can I calculate the accuracy of my system?
The thing is that I also found the following paper on page 2. It uses arcSin() to calculate the angle resolution
http://www.nxp.com/files/sensors/doc/app_note/AN3107.pdf
It calculates the resolution in a different way and I get confused which method is correct.