Hi All,
First let me brief the background of my problem.
I am working on a project , where I am collecting data from accelerometer via I2C, filtering the data and then performing calcuations over data. I have timestamped these individual operations and this is what I found out.
Data collection : 1 sample (X,Y,Z) @ 1250Hz, 400HZ I2C clock = 240Micro seconds
Filtering (mathematical implementation of 2nd order butterworth filter) = 460 micro seconds
Calculations over data = 600 micro seconds.
My requirement is that, I need to perform calculations over subsampled data, ( I am sub sampling the 1250 HZ accelerometer data to 50HZ and then performing calculations).
so to get this done, what I have tried to do is.
1. I have placed the functions
get_data() --> functions gets data from accelerometer and
filter_data ()--> functions that filters
in ISR of port1. This will take 700 micro sends.
2. My idea is that when it comes out of ISR, it then goes to calulations().
But the problem is that, the moment the codes enters to ISR msp is resetting.
here is the sections of code.
#pragma vector = PORT2_VECTOR
__interrupt void P2_ISR(void)
{
// Temporary register
volatile uint8_t Mask_ , Mask_2;
/********************************************************************************************************************/
/****************************************** Accelerometer interrupt request?*****************************************/
/********************************************************************************************************************/
Mask_ = P2IFG & MASK2;
if( Mask_ ) // LIS3DH IRQ
{
//Event |= EventAccelerometer;
_H;
get_accel_data(); //906micro seconds no writing to flash yet
if(++local > 1251)
{
InitLis3dh_4_data(0);
_nop();
_L;
}
}
/********************************************************************************************************************/
/******************************************* Clear interrupt flags **************************************************/
/********************************************************************************************************************/
P2IFG = 0x00;
// Set an active mode on ISR exit, CPU needs to be active to take the proper actions
_low_power_mode_off_on_exit( );
}//P2_ISR
void get_accel_data (void)
{
Bu_16[0] = Bu_16[1] = Bu_16[2] = 0x0000;
//get_data_zone ~~~~~~~~~~~~~~~~~~~ 240 micro seconds Start
Bu_[0] = 0xA8;
I2CWrite( LIS3DH_ADDR , Bu_ , 1 );
I2CRead ( LIS3DH_ADDR , Bu_ , 6 );
data[0] = ((Bu_16[0] + Bu_[1]) << 8) + Bu_[0] ;
data[1] = ((Bu_16[1] + Bu_[3]) << 8) + Bu_[2] ;
data[2] = ((Bu_16[2] + Bu_[5]) << 8) + Bu_[4] ;
//get_data_zone ~~~~~~~~~~~~~~~~~~~ 240 micro seconds END
filter(data); // 460 micro seconds
}
void filter(float *value)
{
xa[0] = xa[1]; ya[0] = ya[1];za[0] = za[1];
xa[1] = xa[2]; ya[1] = ya[2];za[1] = za[2];
//
x_raw = *value;
y_raw = *(value + 1);
z_raw = *(value + 2);
out_buffer[0] = (int)*(value+2);
//all the below 60 micro seconds
xa[2] = *value / 195;
ya[2] = *(value+1) / 195;
za[2] = *(value+2) / 195;
//
xb[0] = xb[1];yb[0] = yb[1];zb[0] = zb[1];
xb[1] = xb[2];yb[1] = yb[2];zb[1] = zb[2];
//
// if(filter_seeding < 3)
// {
// filter_seeding = filter_seeding + 1;
// xb[2] = x_raw;
// yb[2] = y_raw;
// zb[2] = z_raw;
// }else{
//
x_raw_sum = xa[0] + xa[2] + xa[1] + xa[1];
y_raw_sum = ya[0] + ya[2] + ya[1] + ya[1];
z_raw_sum = za[0] + za[2] + za[1] + za[1];
//
x_filter_sum = ( -81 * xb[0]) + ( 179 * xb[1]);
y_filter_sum = ( -81 * yb[0]) + ( 179 * yb[1]);
z_filter_sum = ( -81 * zb[0]) + ( 179 * zb[1]);
//------------------------------------------------------------------------------------------------
if( x_filter_sum < 0)
{
x_convert = -1 * x_filter_sum ;
xb[2] = (x_raw_sum - (float)x_convert /100);
}else
{
x_convert = x_filter_sum ;
xb[2] = (x_raw_sum + (float)x_convert /100);
}
//------------------------------------------------------------------------------------------------
if( y_filter_sum < 0)
{
y_convert = -1 * y_filter_sum ;
yb[2] = ( y_raw_sum - (float)y_convert /100);
}
else
{
y_convert = y_filter_sum ;
yb[2] = ( y_raw_sum + (float)y_convert /100);
}
//------------------------------------------------------------------------------------------------
if( z_filter_sum < 0)
{
z_convert = -1 * z_filter_sum ;
zb[2] = ( z_raw_sum - (float)z_convert /100);
}
else
{
z_convert = z_filter_sum ;
zb[2] = ( z_raw_sum + (float)z_convert /100);
}
//------------------------------------------------------------------------------------------------
//
LP_X_Buff[5] = xb[2] ;
LP_Y_Buff[5] = yb[2] ;
LP_Z_Buff[5] = zb[2] ;
//
// }
//out_buffer[1] = (int) (zb[2]);
if(++_50HZ == 26){
//P1OUT |= BIT2;
MD_engine(); //600 micro seconds
_50HZ = 0;
//P1OUT &= ~BIT2;
}
}