Other Parts Discussed in Thread: MSP430F47197
There is an uncertainty in here. Do I need to set my PINS to I2C mode according to the datasheet of MSP430F47197 or just set the Clock and Data right for the EEPROM?
CPU + EEPROM
Datasheet
Because we have RE/WR functions for EEPROm ready in the workspace but I am not quite sure that we need to use P2.2 and P2.1 for the I2C mode or not!
Workspace
We also have an I2C C file that communicates with the device with I2C capability.
So, now my confusion is Do I need to use something like 208 + my Wr/Re function?
This is really confusing and in either way it is not reading back from the EEPROM IC.
Any idea please?