Two days ago I've bought a now eZ430-Chronos watch and tried to program on it. I've just loaded a sample code into it. The file seems to be loaded in successfully but then, it seems I've flashed all its features aways and now there shows nothing on the screen.
This is the sample code I've compiled and loaded:
#include "cc430x613x.h"
#define Num_of_Results 8
volatile unsigned int A0results[Num_of_Results];
volatile unsigned int A1results[Num_of_Results];
volatile unsigned int A2results[Num_of_Results];
volatile unsigned int A3results[Num_of_Results];
void main(void)
{
WDTCTL = WDTPW+WDTHOLD; // Stop watchdog timer
P2SEL = 0x0F; // Enable A/D channel inputs
ADC12CTL0 = ADC12ON+ADC12MSC+ADC12SHT0_8; // Turn on ADC12_A, extend sampling time
// to avoid overflow of results
ADC12CTL1 = ADC12SHP+ADC12CONSEQ_3; // Use sampling timer, repeated sequence
ADC12MCTL0 = ADC12INCH_0; // ref+=AVcc, channel = A0
ADC12MCTL1 = ADC12INCH_1; // ref+=AVcc, channel = A1
ADC12MCTL2 = ADC12INCH_2; // ref+=AVcc, channel = A2
ADC12MCTL3 = ADC12INCH_3+ADC12EOS; // ref+=AVcc, channel = A3, end seq.
ADC12IE = 0x08; // Enable ADC12IFG.3
ADC12CTL0 |= ADC12ENC; // Enable conversions
ADC12CTL0 |= ADC12SC; // Start conversion - software trigger
__bis_SR_register(LPM0_bits + GIE); // Enter LPM0, Enable interrupts
__no_operation(); // For debugger
}
#pragma vector=ADC12_VECTOR
__interrupt void ADC12ISR (void)
{
static unsigned int index = 0;
switch(__even_in_range(ADC12IV,34))
{
case 0: break; // Vector 0: No interrupt
case 2: break; // Vector 2: ADC overflow
case 4: break; // Vector 4: ADC timing overflow
case 6: break; // Vector 6: ADC12IFG0
case 8: break; // Vector 8: ADC12IFG1
case 10: break; // Vector 10: ADC12IFG2
case 12: // Vector 12: ADC12IFG3
A0results[index] = ADC12MEM0; // Move A0 results, IFG is cleared
A1results[index] = ADC12MEM1; // Move A1 results, IFG is cleared
A2results[index] = ADC12MEM2; // Move A2 results, IFG is cleared
A3results[index] = ADC12MEM3; // Move A3 results, IFG is cleared
index++; // Increment results index, modulo; Set Breakpoint1 here
if (index == 8)
index = 0; // Reset index, Set breakpoint 2 here
case 14: break; // Vector 14: ADC12IFG4
case 16: break; // Vector 16: ADC12IFG5
case 18: break; // Vector 18: ADC12IFG6
case 20: break; // Vector 20: ADC12IFG7
case 22: break; // Vector 22: ADC12IFG8
case 24: break; // Vector 24: ADC12IFG9
case 26: break; // Vector 26: ADC12IFG10
case 28: break; // Vector 28: ADC12IFG11
case 30: break; // Vector 30: ADC12IFG12
case 32: break; // Vector 32: ADC12IFG13
case 34: break; // Vector 34: ADC12IFG14
default: break;
}
}