Other Parts Discussed in Thread: MSP430F2011, LM317
Hello!
I am trying to connect a MSP430F2011, placed on a breadboard through spy by wire to the ez430 USB interface. The ez430 is from the eZ430 - RF2500 kit and the uC is just standalone, no board attached. Software wise I am using the IAR Embedded Workbench IDE.
I have created a new workspace and project and loaded a basic example for the F2011, that I got from the site. I have also set up the debugger to "FET Debugger" in project options and selected the MSP430F2011 as the device. When I click debug I get the error:
Failed to load debugee: C:\Documents and Settings\Administrator\My Documents\IAR test\Debug\Exe\test.d43
and popup:
---------------------------
Emulator
---------------------------
Fatal error: Failed to initialize device.
Session aborted!
---------------------------
OK
---------------------------