hy guys,
I have a question what is the difference by including a header file with <...> and "..".
I think when I use the ".." the file have to be in the project folder but I don't where I have to move the files when I use the <...>.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hy guys,
I have a question what is the difference by including a header file with <...> and "..".
I think when I use the ".." the file have to be in the project folder but I don't where I have to move the files when I use the <...>.
Why do you need to use the include with <...>?
Usually the #include directive with <...> is used to include the header files from the compiler folder directory, on the other hand, the #include directive with "..." is used for user implementation files, often located in the folder project or other path informed by user in the build configurations.
Resuming...
If I understand your question, you can find further explanation in the following link: http://stackoverflow.com/questions/3162030/difference-between-angle-bracket-and-double-quotes-while-including-heade
The GCC user manual tell us:
#include <file>This variant is used for system header files. It searches for a file named file in a standard list of system directories. You can prepend directories to this list with the -I option (see Invocation).
#include "file"This variant is used for header files of your own program. It searches for a file named file first in the directory containing the current file, then in the quote directories and then the same directories used for<file>. You can prepend directories to the list of quote directories with the -iquote option.
Regards,
**Attention** This is a public forum