This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I implemented transmitting data via UART using DMA. it works good.
I'm using single transfer.
I want to add the ability to pause and resume the DMA.
Can I simply use DMAEN=0 for suspend and DMAEN = 1 for resume?
after suspending and resuming the DMA, is it will continue transferring from the same source address and size it was at the suspend time?
As shown in figure 11-3, after DMAEN=0, the next transfer will restart from the beginning of the buffer.
[Itsik] - As I see, the size is not reset. I can use it for calculate the location of the next bytes to send - correct?
Table 11-2 shows that TXIFG does not trigger a transfer if TXIE is set. So you could enable the interrupt to pause DMA.
[Itsik] - Yes, but I will have to deal with interrupt handler because it is not promise that I will success to reset the TXIFG after setting the TXIE before the interrupt handler will called. So it looks like little tricky.
If the 1st solution is acceptable I prefer it.
When byte is sent, according to the button state, the register is decremented (Decrement DMAxSZ) and not the local variable (T_Size).
When the DMAEN is reset, the leftmost arrow takes me to the 'Reset' state (Is this state is reset the size register?) then setting back the DMAEN the (DMAxSZ -->T_Size ) register is setting the local value.
So where the size register is reset if the DMA is disabled?
Quota from datasheet:
DMAEN is automatically cleared when DMAxSZ transfers have been made.
According to the datasheet, the DMAEN is reset when the size arrived to zero and not the opposite direction.
For sum up:
Suspend will be implemented by DMAEN = 0;
Resume will be implemented by:
1) calculating the source address using the DMAxSZ value.
2) DMAEN = 1;
3) DMAxSZ with no change.
Can you confirm?
**Attention** This is a public forum