Other Parts Discussed in Thread: CC2541, ADS1293, AFE4403, CC2640, CC2650
I am working on Wireless Heart Monitor with Bluetooth Low Energy, which I would like to modify it in the way that the board would record data (ECG readings) from ADS1293 chip for at least 24 hours and then transfer it over Bluetooth to the Android device (on-demand). According to CC2541 datasheet, it only comes with 8 KB RAM, which I suppose would't be enough for storing such amount of data.
I was wondering if I could replace CC2541 with one of microcontrollers which already support read/write to SD card/Flash? Which MCU should I use? Would you recommend me any better solution?
Any help would be greatly appreciated.