This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello sir,
I using CCS V6 to develop for MSP430F5510.
I need reset vector in fixed address(0x9000).
How to set CCS complier to fixed address for reset vector?
lnk_msp430f5510.cmd
/****************************************************************************/
/* SPECIFY THE SECTIONS ALLOCATION INTO MEMORY */
/****************************************************************************/
SECTIONS
{
.....
SYSNMI : { * ( .int62 ) } > INT62 type = VECT_INIT
.reset : {} > RESET /* MSP430 RESET VECTOR */
}
Thanks.
Dunk Wu said:How to set CCS complier to fixed address for reset vector?
My question is, why do you want to do that?
The power-up reset vector for MSP430F5510 is at 0x0FFFE. Nothing short of re-designing the chip can change that.
**Attention** This is a public forum