This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPWare Version 2.40.00.37: MSP430FR5xx_6xx\mpu.c: MPU_initThreeSegments(): MPUSEG3WE



Hello,
I'm afraid that the RED colored Ws would be Rs. Do you agree?



C:\...\<CCSv61_location>\msp430\MSPWare_2_40_00_37\driverlib\driverlib\MSP430FR5xx_6xx\mpu.c



[Ln.137]

void MPU_initThreeSegments(uint16_t baseAddress,
                           MPU_initThreeSegmentsParam *param)
{
...
[Ln.202]
    // Set access rights based on user's selection for segment3
    switch(param->seg3accmask)
    {
    case MPU_EXEC | MPU_READ:
        HWREG16(baseAddress + OFS_MPUSAM) &= ~MPUSEG3WE;
        HWREG16(baseAddress + OFS_MPUSAM) |= MPUSEG3XE + MPUSEG3RE;
        break;
    case MPU_READ | MPU_WRITE:
        HWREG16(baseAddress + OFS_MPUSAM) &= ~MPUSEG3XE;
        HWREG16(baseAddress + OFS_MPUSAM) |= MPUSEG3RE + MPUSEG3WE;
        break;
    case MPU_READ:
        HWREG16(baseAddress + OFS_MPUSAM) &= ~(MPUSEG3XE + MPUSEG3WE);
        HWREG16(baseAddress + OFS_MPUSAM) |= MPUSEG3RE;
        break;
    case MPU_EXEC | MPU_READ | MPU_WRITE:
        HWREG16(baseAddress +
                OFS_MPUSAM) |= (MPUSEG3XE + MPUSEG3WE + MPUSEG3WE);  /* One of the W would be R ? */
        break;
    case MPU_NO_READ_WRITE_EXEC:
        HWREG16(baseAddress +
                OFS_MPUSAM) &= ~(MPUSEG3XE + MPUSEG3WE + MPUSEG3WE); /* One of the W would be R ? */
        break;
    default:
        break;
    }

    //Lock MPU to disable writing to all registers
    HWREG8(baseAddress + OFS_MPUCTL0_H) = 0x00;
}

**Attention** This is a public forum