Other Parts Discussed in Thread: CC430F5137
I have a problem reading any data in SPI slave mode on CC430F5137 mC. As a master I use Raspberry Pi 2. Pi is configured correctly and sends correct data (I checked this with oscilloscope). mC do not read any data though. I do not matter ho I configure SPI on mC (clock polarity, phase etc.). I though that it may be problem with 5V Vcc and 3.3V Vcc difference in Pi and mC and used 2 way logic level converter in between but it still do not changed anything. I think speed is also not an issue since 1MHz surely is in capabilities of both devices. I checked physical connections - fine too. The only other thing that might be wrong is software on mC. Here i a code I use:
uint8_t transmitData = 0x01, receiveData = 0x00;
uint8_t returnValue = STATUS_FAIL;
void prog_main(void)
{
//Stop watchdog timer
WDT_A_hold(WDT_A_BASE);
//If clock signal from master stays low, it is not yet in SPI mode
while ( GPIO_INPUT_PIN_LOW ==
GPIO_getInputPinValue(
GPIO_PORT_P1,
GPIO_PIN4
)) ;
GPIO_setAsPeripheralModuleFunctionInputPin(
GPIO_PORT_P1,
GPIO_PIN2 +
GPIO_PIN3 + GPIO_PIN4 + GPIO_PIN7
);
returnValue = USCI_B_SPI_slaveInit(USCI_B0_BASE,
USCI_B_SPI_MSB_FIRST,
USCI_B_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT
USCI_B_SPI_CLOCKPOLARITY_INACTIVITY_LOW
);
if (STATUS_FAIL == returnValue)
return;
//Enable SPI Module
USCI_B_SPI_enable(USCI_B0_BASE);
//Enable Receive interrupt
USCI_B_SPI_clearInterruptFlag(USCI_B0_BASE,
USCI_B_SPI_RECEIVE_INTERRUPT
);
USCI_B_SPI_enableInterrupt(USCI_B0_BASE,
USCI_B_SPI_RECEIVE_INTERRUPT
);
//Enter LPM4, enable interrupts
__bis_SR_register(
LPM4_bits +
GIE);
}
uint8_t a=0;
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_B0_VECTOR
__interrupt
#elif defined(__GNUC__)
__attribute__((interrupt(USCI_B0_VECTOR)))
#endif
void USCI_B0_ISR(void)
{
switch (__even_in_range(UCB0IV, 4)) {
//Vector 2 - RXIFG
case 2:
//USCI_A0 TX buffer ready?
while (!USCI_B_SPI_getInterruptStatus(USCI_B0_BASE,
USCI_B_SPI_TRANSMIT_INTERRUPT
));
//Transmit data to master
USCI_B_SPI_transmitData(USCI_B0_BASE,
transmitData
);
//Receive data from master
receiveData = USCI_B_SPI_receiveData(USCI_B0_BASE);
if(receiveData!=0)
{
//Increment data to be transmitted
transmitData++;
}
break;
default: break;
}
}