Other Parts Discussed in Thread: MSP430F67791, MSP430F6779
Hi All,
someone know the ram amount usage of the aes-gcm 128 http://downloads.ti.com/tsu_encryption/tsu_encryption_public_sw
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F67791, MSP430F6779
Hi All,
someone know the ram amount usage of the aes-gcm 128 http://downloads.ti.com/tsu_encryption/tsu_encryption_public_sw
Hi Sean,
thanks for your reply.
I would like to use the algorithm on msp430 with 16 KB ram as you can imagine i need to know the amount of the aes-gcm ram usage in order to verify all the other things ram allocated.
Do you know that amount ?
Thanks in advance
Reg.
Fabio
Hi Fabio,
Here is an idea to check RAM usage of the source code on your device. When you build the project a *.map file is created - it is a memory map where you can check what memory sections you are using. Below is a snippet of my map file for a sample program.
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
SFR 00000000 00000010 00000000 00000010 RWIX
PERIPHERALS_8BIT 00000010 000000f0 00000000 000000f0 RWIX
PERIPHERALS_16BIT 00000100 00000100 00000000 00000100 RWIX
INFOA 00001c00 00000060 00000000 00000060 RWIX
INT00 00001c60 00000002 00000000 00000002 RWIX
INT01 00001c62 00000002 00000000 00000002 RWIX
INT02 00001c64 00000002 00000000 00000002 RWIX
INT03 00001c66 00000002 00000000 00000002 RWIX
INT04 00001c68 00000002 00000000 00000002 RWIX
INT05 00001c6a 00000002 00000002 00000000 RWIX
INT06 00001c6c 00000002 00000002 00000000 RWIX
INT07 00001c6e 00000002 00000002 00000000 RWIX
INT08 00001c70 00000002 00000002 00000000 RWIX
INT09 00001c72 00000002 00000002 00000000 RWIX
INT10 00001c74 00000002 00000002 00000000 RWIX
INT11 00001c76 00000002 00000002 00000000 RWIX
INT12 00001c78 00000002 00000002 00000000 RWIX
INT13 00001c7a 00000002 00000002 00000000 RWIX
INT14 00001c7c 00000002 00000002 00000000 RWIX
RESET 00001c7e 00000002 00000002 00000000 RWIX
FLASH 00001c80 00000700 00000064 0000069c RWIX
RAM 00002380 00000080 00000050 00000030 RWIX
Therefore, I suggest building the AES GCM source code on your particular MSP430 device and checking the memory configuration.
Sincerely,
Sean
**Attention** This is a public forum