Other Parts Discussed in Thread: MSP430F5529, MSP-TS430PN80USB
Hello,
I'm having trouble connecting to my MSP430F5529 (sitting on the MSP-TS430PN80USB development board) using the MSP FET. I've installed CCSv6.1.2, and all the drivers for the MSP FET seem to have installed properly. When I connect the MSP FET to my computer via USB, the green LED stays lit on the MSP FET, and my Windows Device Manager (Windows 10) seems to properly detect the hardware and load the appropriate driver.
When I try to start a new project in CCS to run the 'Hello World' example to blink the LED on the development board, it won't let me identify the target. CCS just hangs on the popup saying "Starting Debug Server..." It continues to hang until I unplug the USB cable, at which time it shows an error message saying there was a communication error.
I've also installed CCSv6 on an Ubuntu system and had the same problems.
I've tried searching through similar problems in the forums, but none of the solutions there seemed to help (update drivers, re-install CCS, try another computer, etc...)
Any help or redirection to another post would be greatly appreciated.
Cheers,
Mike