This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
I was trying to interface G2553 with another guy. But the problem is another guy is completely packed and he doesn't have any space through which I can talk, except an ADC input channel.
So, I was wondering If there is a way I can get the temperature sensor analog out on any of those pins of g2553? And wire it to analog channel of another guy?
Thanks in advance!
Making your own DAC could be done if the msp430 still have a TA0.1 or TA0.2 TA1.1 or TA1.2 pin available.
resistor and a cap to create a filter.
But surely the other "guy" must have the option to set the ADC pin as general GPIO?
If so just create a single-wire-protocol to send 10bit data.
is there no i2c bus you can tap in to?
To be honest - to use msp430 as _analog_ temperature sensor is total waste, especially knowing that it's built-in temperature sensor is not that good at all. Note that absolute precision of it is not even specified. Why don't you simply use temperature sensor IC with analog output? TI have plenty to choose from
**Attention** This is a public forum