Other Parts Discussed in Thread: MSP430F5529
The MSP430x5xx Family User’s Manual states…
For a given DCO bias range setting, time must be allowed for the DCO to settle on the proper tap for normal operation. (n × 32) fFLLREFCLK cycles are required between taps requiring a worst case of (n × 32 × 32) fFLLREFCLK cycles for the DCO to settle. The value n is defined by the FLLREFDIV bits (n = 1, 2, 4, 8, 12, or 16).
Several of the examples in ‘F552x_C_Code_Examples’ include the delay…
__bic_SR_register(SCG0); // Enable the FLL control loop
// Worst-case settling time for the DCO when the DCO range bits have been
// changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
// UG for optimization.
// 32 x 32 x 2.45 MHz / 32,768 Hz = 76563 = MCLK cycles for DCO to settle
__delay_cycles(76563);
// Loop until XT1,XT2 & DCO fault flag is cleared
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + XT1HFOFFG + DCOFFG);
// Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
While the ‘void Init_FLL(const unsigned int fsystem, const unsigned int ratio)’ function in ‘hal_USC.C’ does not.
Delay or not?
Thanks,
Steve