This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NFC and Capacitive Touch in the Same MCU

Other Parts Discussed in Thread: MSP430FR2633, DLP-7970ABP, MSP430F5529

Are there any processors for which TI has NFC software to interface toe the TRF7970 and that have support for cap touch sensor buttons?

  • One example is the MSP430F5529. If you refer to the MSP-EXP430F5529, then you will find examples for the NFC and capacitive touch. Alternatively you could use the CapTIvate library/dev kit for the MSP430FR2633 and the DLP-7970ABP boosterpack, but you would need to port the boosterpack MCU firmware to the FR2633.

    Some things to consider are the type of NFC support you need (basic reader/writer, full, peer-to-peer, card emulation, compliance) which will directly relate to the code size and available platforms.

    Regards,
    Chris

**Attention** This is a public forum