This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reading temperature of MSP430

Hello,

The following code enables to read working temperature of the MCU.

Is it possible to read without using interrupt but by polling end of sampling ?

#include <msp430f5529.h>

long temp;

/****************************************************************************************/
int mcu_read_temperature (long *Temp)
{
	REFCTL0 &= ~REFMSTR;                      			// Reset REFMSTR to hand over control to ADC12_A ref control registers
	ADC12CTL0 = ADC12SHT0_8 + ADC12REFON + ADC12ON; 	// Internal ref = 1.5V
	ADC12CTL1 = ADC12SHP;                     			// enable sample timer
	ADC12MCTL0 = ADC12SREF_1 + ADC12INCH_10;  			// ADC i/p ch A10 = temp sense i/p
	ADC12IE = 0x001;                          			// ADC_IFG upon conv result-ADCMEMO

	ADC12CTL0 |= ADC12ENC;

	ADC12CTL0 |= ADC12SC;                   			// Sampling and conversion start

	*Temp = ((temp - 1830) * 546) / 4096;

	return 0;
}

/****************************************************************************************/
#pragma vector=ADC12_VECTOR
__interrupt void ADC12ISR (void)
{
  switch(__even_in_range(ADC12IV,34))
  {
  case  0: break;                           // Vector  0:  No interrupt
  case  2: break;                           // Vector  2:  ADC overflow
  case  4: break;                           // Vector  4:  ADC timing overflow
  case  6:                                  // Vector  6:  ADC12IFG0
    temp = ADC12MEM0;                       // Move results, IFG is cleared
//    __bic_SR_register_on_exit(LPM4_bits);   // Exit active CPU
  case  8: break;                           // Vector  8:  ADC12IFG1
  case 10: break;                           // Vector 10:  ADC12IFG2
  case 12: break;                           // Vector 12:  ADC12IFG3
  case 14: break;                           // Vector 14:  ADC12IFG4
  case 16: break;                           // Vector 16:  ADC12IFG5
  case 18: break;                           // Vector 18:  ADC12IFG6
  case 20: break;                           // Vector 20:  ADC12IFG7
  case 22: break;                           // Vector 22:  ADC12IFG8
  case 24: break;                           // Vector 24:  ADC12IFG9
  case 26: break;                           // Vector 26:  ADC12IFG10
  case 28: break;                           // Vector 28:  ADC12IFG11
  case 30: break;                           // Vector 30:  ADC12IFG12
  case 32: break;                           // Vector 32:  ADC12IFG13
  case 34: break;                           // Vector 34:  ADC12IFG14
  default: break;
  }
}


Best regards,
Z.V

**Attention** This is a public forum